public class RoutingBulkReplacementBuilderRetainReasonType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BLOCK_UNIFY
Retain reason is because of the presence of the NX_BLOCK_UNIFY attribute
|
static int |
_EQUIPMENT
Retain reason is the object is equipment and is not supported
|
static int |
_EXPLICIT
Retain reason is the user explicitly marked it retain
|
static int |
_NON_CLASSIFICATION
Retain reason is the object did not originate from classification and is not supported
|
static int |
_UNSPECIFIED
Retain reason is not specified
|
static RoutingBulkReplacementBuilderRetainReasonType |
BLOCK_UNIFY
Retain reason is because of the presence of the NX_BLOCK_UNIFY attribute
|
static RoutingBulkReplacementBuilderRetainReasonType |
EQUIPMENT
Retain reason is the object is equipment and is not supported
|
static RoutingBulkReplacementBuilderRetainReasonType |
EXPLICIT
Retain reason is the user explicitly marked it retain
|
static RoutingBulkReplacementBuilderRetainReasonType |
NON_CLASSIFICATION
Retain reason is the object did not originate from classification and is not supported
|
static RoutingBulkReplacementBuilderRetainReasonType |
UNSPECIFIED
Retain reason is not specified
|
Modifier and Type | Method and Description |
---|---|
static RoutingBulkReplacementBuilderRetainReasonType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingBulkReplacementBuilderRetainReasonType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingBulkReplacementBuilderRetainReasonType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RoutingBulkReplacementBuilderRetainReasonType UNSPECIFIED
public static final RoutingBulkReplacementBuilderRetainReasonType EXPLICIT
public static final RoutingBulkReplacementBuilderRetainReasonType BLOCK_UNIFY
public static final RoutingBulkReplacementBuilderRetainReasonType NON_CLASSIFICATION
public static final RoutingBulkReplacementBuilderRetainReasonType EQUIPMENT
public static final int _UNSPECIFIED
public static final int _EXPLICIT
public static final int _BLOCK_UNIFY
public static final int _NON_CLASSIFICATION
public static final int _EQUIPMENT
public static RoutingBulkReplacementBuilderRetainReasonType valueOf(int value)
public static RoutingBulkReplacementBuilderRetainReasonType valueOf(String name)
public static RoutingBulkReplacementBuilderRetainReasonType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.