Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
RoutingBulkReplacementBuilderLibrarySelectSourceType.CLASSIFICATION
Library select source is a classification object
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
RoutingBulkReplacementBuilderLibrarySelectSourceType.SPECIFIC_PART
Library select source is a specific part
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
RoutingBulkReplacementBuilderLibrarySelectSourceType.UNSPECIFIED
Library select source is not specified
|
Modifier and Type | Method and Description |
---|---|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
RoutingBulkReplacementBuilderLibrarySelectSourceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
RoutingBulkReplacementBuilderLibrarySelectSourceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType[] |
RoutingBulkReplacementBuilderLibrarySelectSourceType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.