public class RoutingBulkReplacementBuilderLibrarySelectSourceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CLASSIFICATION
Library select source is a classification object
|
static int |
_SPECIFIC_PART
Library select source is a specific part
|
static int |
_UNSPECIFIED
Library select source is not specified
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
CLASSIFICATION
Library select source is a classification object
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
SPECIFIC_PART
Library select source is a specific part
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
UNSPECIFIED
Library select source is not specified
|
Modifier and Type | Method and Description |
---|---|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingBulkReplacementBuilderLibrarySelectSourceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RoutingBulkReplacementBuilderLibrarySelectSourceType UNSPECIFIED
public static final RoutingBulkReplacementBuilderLibrarySelectSourceType CLASSIFICATION
public static final RoutingBulkReplacementBuilderLibrarySelectSourceType SPECIFIC_PART
public static final int _UNSPECIFIED
public static final int _CLASSIFICATION
public static final int _SPECIFIC_PART
public static RoutingBulkReplacementBuilderLibrarySelectSourceType valueOf(int value)
public static RoutingBulkReplacementBuilderLibrarySelectSourceType valueOf(String name)
public static RoutingBulkReplacementBuilderLibrarySelectSourceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.