Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static PlatformCreatorBuilder.ReferenceType |
PlatformCreatorBuilder.ReferenceType.HORIZONTAL |
static PlatformCreatorBuilder.ReferenceType |
PlatformCreatorBuilder.ReferenceType.VERTICAL |
Modifier and Type | Method and Description |
---|---|
PlatformCreatorBuilder.ReferenceType |
PlatformCreatorBuilder.grateOrientationReference()
Returns the grate orientation reference
License requirements: routing_platform ("Routing Platform") . |
static PlatformCreatorBuilder.ReferenceType |
PlatformCreatorBuilder.ReferenceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformCreatorBuilder.ReferenceType |
PlatformCreatorBuilder.ReferenceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformCreatorBuilder.ReferenceType[] |
PlatformCreatorBuilder.ReferenceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlatformCreatorBuilder.setGrateOrientationReference(PlatformCreatorBuilder.ReferenceType grateOrientationReference)
License requirements: routing_platform ("Routing Platform") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.