public static class PlatformCreatorBuilder.ReferenceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL |
static int |
_VERTICAL |
static PlatformCreatorBuilder.ReferenceType |
HORIZONTAL |
static PlatformCreatorBuilder.ReferenceType |
VERTICAL |
Modifier and Type | Method and Description |
---|---|
static PlatformCreatorBuilder.ReferenceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformCreatorBuilder.ReferenceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformCreatorBuilder.ReferenceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlatformCreatorBuilder.ReferenceType HORIZONTAL
public static final PlatformCreatorBuilder.ReferenceType VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static PlatformCreatorBuilder.ReferenceType valueOf(int value)
public static PlatformCreatorBuilder.ReferenceType valueOf(String name)
public static PlatformCreatorBuilder.ReferenceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.