Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CustomManager.PipingComponentFileOptions |
CustomManager.PipingComponentFileOptions.ALWAYS_OVERWRITE_FILE
Always overwrite any existing piping component file.
|
static CustomManager.PipingComponentFileOptions |
CustomManager.PipingComponentFileOptions.ASK_TO_OVERWRITE_FILE
Prompt the user of the plugin if it is OK to overwrite the piping component file.
|
static CustomManager.PipingComponentFileOptions |
CustomManager.PipingComponentFileOptions.NEVER_OVERWRITE_FILE
Never overwrite any existing piping component file.
|
Modifier and Type | Method and Description |
---|---|
static CustomManager.PipingComponentFileOptions |
CustomManager.PipingComponentFileOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.PipingComponentFileOptions |
CustomManager.PipingComponentFileOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.PipingComponentFileOptions[] |
CustomManager.PipingComponentFileOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomManager.PipingComponentFilePlugin.pipingComponentFilePlugin(String fileName,
Component[] components,
CustomManager.PipingComponentFileOptions options)
This defines the prototype for the piping component file plugin.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.