public static class CustomManager.PipingComponentFileOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALWAYS_OVERWRITE_FILE
Always overwrite any existing piping component file.
|
static int |
_ASK_TO_OVERWRITE_FILE
Prompt the user of the plugin if it is OK to overwrite the piping component file.
|
static int |
_NEVER_OVERWRITE_FILE
Never overwrite any existing piping component file.
|
static CustomManager.PipingComponentFileOptions |
ALWAYS_OVERWRITE_FILE
Always overwrite any existing piping component file.
|
static CustomManager.PipingComponentFileOptions |
ASK_TO_OVERWRITE_FILE
Prompt the user of the plugin if it is OK to overwrite the piping component file.
|
static CustomManager.PipingComponentFileOptions |
NEVER_OVERWRITE_FILE
Never overwrite any existing piping component file.
|
Modifier and Type | Method and Description |
---|---|
static CustomManager.PipingComponentFileOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.PipingComponentFileOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.PipingComponentFileOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final CustomManager.PipingComponentFileOptions ASK_TO_OVERWRITE_FILE
public static final CustomManager.PipingComponentFileOptions NEVER_OVERWRITE_FILE
public static final CustomManager.PipingComponentFileOptions ALWAYS_OVERWRITE_FILE
public static final int _ASK_TO_OVERWRITE_FILE
public static final int _NEVER_OVERWRITE_FILE
public static final int _ALWAYS_OVERWRITE_FILE
public static CustomManager.PipingComponentFileOptions valueOf(int value)
public static CustomManager.PipingComponentFileOptions valueOf(String name)
public static CustomManager.PipingComponentFileOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.