Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
CustomManager.DuctSizeCalculatorDisplayNoteFlag.ADD_NOTE |
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
CustomManager.DuctSizeCalculatorDisplayNoteFlag.REMOVE_NOTE |
Modifier and Type | Method and Description |
---|---|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
CustomManager.DuctSizeCalculatorDisplayNoteFlag.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
CustomManager.DuctSizeCalculatorDisplayNoteFlag.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag[] |
CustomManager.DuctSizeCalculatorDisplayNoteFlag.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomManager.DuctSizeCalculatorDisplayNotePlugin.ductSizeCalculatorDisplayNotePlugin(Curve segment,
CustomManager.DuctSizeCalculatorDisplayNoteFlag displayOrRemove)
This defines the prototype for the Duct Size Calculator's Display Note plugin.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.