public static class CustomManager.DuctSizeCalculatorDisplayNoteFlag extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD_NOTE |
static int |
_REMOVE_NOTE |
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
ADD_NOTE |
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
REMOVE_NOTE |
Modifier and Type | Method and Description |
---|---|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.DuctSizeCalculatorDisplayNoteFlag[] |
values()
Returns an array that contains the values for this enum.
|
public static final CustomManager.DuctSizeCalculatorDisplayNoteFlag ADD_NOTE
public static final CustomManager.DuctSizeCalculatorDisplayNoteFlag REMOVE_NOTE
public static final int _ADD_NOTE
public static final int _REMOVE_NOTE
public static CustomManager.DuctSizeCalculatorDisplayNoteFlag valueOf(int value)
public static CustomManager.DuctSizeCalculatorDisplayNoteFlag valueOf(String name)
public static CustomManager.DuctSizeCalculatorDisplayNoteFlag[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.