Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static BendCornerCollection.Type |
BendCornerCollection.Type.RADIUS_RATIO
Using radius or ratio to
create a bend corner.
|
static BendCornerCollection.Type |
BendCornerCollection.Type.TABLE
Using a bend table to create a
bend corner.
|
Modifier and Type | Method and Description |
---|---|
static BendCornerCollection.Type |
BendCornerCollection.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendCornerCollection.Type |
BendCornerCollection.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendCornerCollection.Type[] |
BendCornerCollection.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.