public static class BendCornerCollection.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RADIUS_RATIO
Using radius or ratio to
create a bend corner.
|
static int |
_TABLE
Using a bend table to create a
bend corner.
|
static BendCornerCollection.Type |
RADIUS_RATIO
Using radius or ratio to
create a bend corner.
|
static BendCornerCollection.Type |
TABLE
Using a bend table to create a
bend corner.
|
Modifier and Type | Method and Description |
---|---|
static BendCornerCollection.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendCornerCollection.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendCornerCollection.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final BendCornerCollection.Type RADIUS_RATIO
public static final BendCornerCollection.Type TABLE
public static final int _RADIUS_RATIO
public static final int _TABLE
public static BendCornerCollection.Type valueOf(int value)
public static BendCornerCollection.Type valueOf(String name)
public static BendCornerCollection.Type[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.