Package | Description |
---|---|
nxopen.presslinesimulation |
Provides classes and interfaces for Press Line Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MountPointBuilder.GeometrySelectionFilterType |
MountPointBuilder.GeometrySelectionFilterType.ALL
Everything can be selected.
|
static MountPointBuilder.GeometrySelectionFilterType |
MountPointBuilder.GeometrySelectionFilterType.ONLY_UNMOUNTED
Only bodies that are not mounted can be selected.
|
Modifier and Type | Method and Description |
---|---|
MountPointBuilder.GeometrySelectionFilterType |
MountPointBuilder.selectionFilter()
Returns the geometry selection filter
License requirements: None. |
static MountPointBuilder.GeometrySelectionFilterType |
MountPointBuilder.GeometrySelectionFilterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MountPointBuilder.GeometrySelectionFilterType |
MountPointBuilder.GeometrySelectionFilterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MountPointBuilder.GeometrySelectionFilterType[] |
MountPointBuilder.GeometrySelectionFilterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MountPointBuilder.setSelectionFilter(MountPointBuilder.GeometrySelectionFilterType selectionFilter)
License requirements: nx_pls_die_checker (" NX Press Die Checker") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.