public static class MountPointBuilder.GeometrySelectionFilterType extends Enum
MountPointBuilder.selectionFilter()
and MountPointBuilder.setSelectionFilter(nxopen.presslinesimulation.MountPointBuilder.GeometrySelectionFilterType)
to
filter the selectable items that should be mounted.Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Everything can be selected.
|
static int |
_ONLY_UNMOUNTED
Only bodies that are not mounted can be selected.
|
static MountPointBuilder.GeometrySelectionFilterType |
ALL
Everything can be selected.
|
static MountPointBuilder.GeometrySelectionFilterType |
ONLY_UNMOUNTED
Only bodies that are not mounted can be selected.
|
Modifier and Type | Method and Description |
---|---|
static MountPointBuilder.GeometrySelectionFilterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MountPointBuilder.GeometrySelectionFilterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MountPointBuilder.GeometrySelectionFilterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MountPointBuilder.GeometrySelectionFilterType ONLY_UNMOUNTED
public static final MountPointBuilder.GeometrySelectionFilterType ALL
public static final int _ONLY_UNMOUNTED
public static final int _ALL
public static MountPointBuilder.GeometrySelectionFilterType valueOf(int value)
public static MountPointBuilder.GeometrySelectionFilterType valueOf(String name)
public static MountPointBuilder.GeometrySelectionFilterType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.