Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.DeleteChildFeaturesOptionType.ASK
Ask user "Do you want to delete child features?"
|
static SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.DeleteChildFeaturesOptionType.NO
Do not delete child features of feature being deleted
|
static SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.DeleteChildFeaturesOptionType.YES
Delete child features including recipe curves, of a feature being deleted
|
Modifier and Type | Method and Description |
---|---|
SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.deleteChildFeaturesOption()
Returns the delete child features options
License requirements: None. |
static SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.DeleteChildFeaturesOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.DeleteChildFeaturesOptionType |
SessionModeling.DeleteChildFeaturesOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.DeleteChildFeaturesOptionType[] |
SessionModeling.DeleteChildFeaturesOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionModeling.setDeleteChildFeaturesOption(SessionModeling.DeleteChildFeaturesOptionType deleteChildFeatureOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.