public static class SessionModeling.DeleteChildFeaturesOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ASK
Ask user "Do you want to delete child features?"
|
static int |
_NO
Do not delete child features of feature being deleted
|
static int |
_YES
Delete child features including recipe curves, of a feature being deleted
|
static SessionModeling.DeleteChildFeaturesOptionType |
ASK
Ask user "Do you want to delete child features?"
|
static SessionModeling.DeleteChildFeaturesOptionType |
NO
Do not delete child features of feature being deleted
|
static SessionModeling.DeleteChildFeaturesOptionType |
YES
Delete child features including recipe curves, of a feature being deleted
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.DeleteChildFeaturesOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.DeleteChildFeaturesOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.DeleteChildFeaturesOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.DeleteChildFeaturesOptionType YES
public static final SessionModeling.DeleteChildFeaturesOptionType NO
public static final SessionModeling.DeleteChildFeaturesOptionType ASK
public static final int _YES
public static final int _NO
public static final int _ASK
public static SessionModeling.DeleteChildFeaturesOptionType valueOf(int value)
public static SessionModeling.DeleteChildFeaturesOptionType valueOf(String name)
public static SessionModeling.DeleteChildFeaturesOptionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.