Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Method and Description |
---|---|
PmiOption |
InheritPmiViewStyle.inheritPmiMode()
Returns the Inherit pmi mode.
|
PmiOption |
ViewStyleInheritPmiBuilder.pmi()
Returns the pmi option on the INHERIT PMI tab of the View Style Dialog
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
InheritPmiViewStyle.setInheritPmiMode(PmiOption pmiOption)
License requirements: drafting ("DRAFTING") . |
void |
ViewStyleInheritPmiBuilder.setPmi(PmiOption pmiOption)
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Field and Description |
---|---|
static PmiOption |
PmiOption.FROM_MODEL_VIEW
Inherit PMI from the parent model view.
|
static PmiOption |
PmiOption.IN_DRAWING_PLANE_FROM_PART
Inherit PMI that are parallel to the drawing plane from the entire part.
|
static PmiOption |
PmiOption.IN_DRAWING_PLANE_FROM_VIEW
Inherit PMI that are parallel to the drawing plane from the model view.
|
static PmiOption |
PmiOption.NONE
Does not inherit PMI.
|
Modifier and Type | Method and Description |
---|---|
PmiOption |
InheritPmiPreferences.inheritPmiMode()
Returns the Status of inherit pmi mode.
|
static PmiOption |
PmiOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PmiOption |
PmiOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PmiOption[] |
PmiOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InheritPmiPreferences.setInheritPmiMode(PmiOption pmiOption)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.