public class PmiOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_MODEL_VIEW
Inherit PMI from the parent model view.
|
static int |
_IN_DRAWING_PLANE_FROM_PART
Inherit PMI that are parallel to the drawing plane from the entire part.
|
static int |
_IN_DRAWING_PLANE_FROM_VIEW
Inherit PMI that are parallel to the drawing plane from the model view.
|
static int |
_NONE
Does not inherit PMI.
|
static PmiOption |
FROM_MODEL_VIEW
Inherit PMI from the parent model view.
|
static PmiOption |
IN_DRAWING_PLANE_FROM_PART
Inherit PMI that are parallel to the drawing plane from the entire part.
|
static PmiOption |
IN_DRAWING_PLANE_FROM_VIEW
Inherit PMI that are parallel to the drawing plane from the model view.
|
static PmiOption |
NONE
Does not inherit PMI.
|
Modifier and Type | Method and Description |
---|---|
static PmiOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PmiOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PmiOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PmiOption NONE
public static final PmiOption FROM_MODEL_VIEW
public static final PmiOption IN_DRAWING_PLANE_FROM_VIEW
public static final PmiOption IN_DRAWING_PLANE_FROM_PART
public static final int _NONE
public static final int _FROM_MODEL_VIEW
public static final int _IN_DRAWING_PLANE_FROM_VIEW
public static final int _IN_DRAWING_PLANE_FROM_PART
public static PmiOption valueOf(int value)
public static PmiOption valueOf(String name)
public static PmiOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.