Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.GM_PER_CU_CM
Unit is gram per cubic centimeter
|
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.KG_PER_CU_METER
Unit is kg per cubic meter
|
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.LB_PER_CU_FEET
Unit is pound per cubic feet
|
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.LB_PER_CU_INCH
Unit is pound per cubic inch
|
Modifier and Type | Method and Description |
---|---|
PartModeling.DensityUnitType |
PartModeling.densityUnit()
Returns the density unit
License requirements: None. |
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartModeling.DensityUnitType |
PartModeling.DensityUnitType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartModeling.DensityUnitType[] |
PartModeling.DensityUnitType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartModeling.setDensityUnit(PartModeling.DensityUnitType densityUnit)
Sets the density unit
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.