public static class PartModeling.DensityUnitType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GM_PER_CU_CM
Unit is gram per cubic centimeter
|
static int |
_KG_PER_CU_METER
Unit is kg per cubic meter
|
static int |
_LB_PER_CU_FEET
Unit is pound per cubic feet
|
static int |
_LB_PER_CU_INCH
Unit is pound per cubic inch
|
static PartModeling.DensityUnitType |
GM_PER_CU_CM
Unit is gram per cubic centimeter
|
static PartModeling.DensityUnitType |
KG_PER_CU_METER
Unit is kg per cubic meter
|
static PartModeling.DensityUnitType |
LB_PER_CU_FEET
Unit is pound per cubic feet
|
static PartModeling.DensityUnitType |
LB_PER_CU_INCH
Unit is pound per cubic inch
|
Modifier and Type | Method and Description |
---|---|
static PartModeling.DensityUnitType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartModeling.DensityUnitType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartModeling.DensityUnitType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartModeling.DensityUnitType LB_PER_CU_INCH
public static final PartModeling.DensityUnitType LB_PER_CU_FEET
public static final PartModeling.DensityUnitType GM_PER_CU_CM
public static final PartModeling.DensityUnitType KG_PER_CU_METER
public static final int _LB_PER_CU_INCH
public static final int _LB_PER_CU_FEET
public static final int _GM_PER_CU_CM
public static final int _KG_PER_CU_METER
public static PartModeling.DensityUnitType valueOf(int value)
public static PartModeling.DensityUnitType valueOf(String name)
public static PartModeling.DensityUnitType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.