Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Field and Description |
---|---|
static Network.ObjectStatus |
Network.ObjectStatus.FIXED
Attempt to put constraint between two fixed objects.
|
static Network.ObjectStatus |
Network.ObjectStatus.NOT_CHANGED
Not evaluated because other parts of the model are over defined or inconsistent.
|
static Network.ObjectStatus |
Network.ObjectStatus.NOT_CONSISTENT_DIMS
Cannot solve with current dimension values.
|
static Network.ObjectStatus |
Network.ObjectStatus.NOT_CONSISTENT_OTHER
Cannot find a solution.
|
static Network.ObjectStatus |
Network.ObjectStatus.NOT_CONSISTENT_UNKNOWN
One movable object fixed.
|
static Network.ObjectStatus |
Network.ObjectStatus.OVER_DEFINED
Conflicts with other constraints.
|
static Network.ObjectStatus |
Network.ObjectStatus.UNDER_DEFINED
The constraint is solved and satisfied
|
static Network.ObjectStatus |
Network.ObjectStatus.UNKNOWN
Not yet evaluated.
|
static Network.ObjectStatus |
Network.ObjectStatus.WELL_DEFINED
The constraint is solved and satisfied
|
Modifier and Type | Method and Description |
---|---|
Network.ObjectStatus |
Network.getMovableObjectStatus(NXObject movableObject)
Returns the solver status of a movable object.
|
static Network.ObjectStatus |
Network.ObjectStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Network.ObjectStatus |
Network.ObjectStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Network.ObjectStatus[] |
Network.ObjectStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.