public static class Network.ObjectStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIXED
Attempt to put constraint between two fixed objects.
|
static int |
_NOT_CHANGED
Not evaluated because other parts of the model are over defined or inconsistent.
|
static int |
_NOT_CONSISTENT_DIMS
Cannot solve with current dimension values.
|
static int |
_NOT_CONSISTENT_OTHER
Cannot find a solution.
|
static int |
_NOT_CONSISTENT_UNKNOWN
One movable object fixed.
|
static int |
_OVER_DEFINED
Conflicts with other constraints.
|
static int |
_UNDER_DEFINED
The constraint is solved and satisfied
|
static int |
_UNKNOWN
Not yet evaluated.
|
static int |
_WELL_DEFINED
The constraint is solved and satisfied
|
static Network.ObjectStatus |
FIXED
Attempt to put constraint between two fixed objects.
|
static Network.ObjectStatus |
NOT_CHANGED
Not evaluated because other parts of the model are over defined or inconsistent.
|
static Network.ObjectStatus |
NOT_CONSISTENT_DIMS
Cannot solve with current dimension values.
|
static Network.ObjectStatus |
NOT_CONSISTENT_OTHER
Cannot find a solution.
|
static Network.ObjectStatus |
NOT_CONSISTENT_UNKNOWN
One movable object fixed.
|
static Network.ObjectStatus |
OVER_DEFINED
Conflicts with other constraints.
|
static Network.ObjectStatus |
UNDER_DEFINED
The constraint is solved and satisfied
|
static Network.ObjectStatus |
UNKNOWN
Not yet evaluated.
|
static Network.ObjectStatus |
WELL_DEFINED
The constraint is solved and satisfied
|
Modifier and Type | Method and Description |
---|---|
static Network.ObjectStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Network.ObjectStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Network.ObjectStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final Network.ObjectStatus UNKNOWN
public static final Network.ObjectStatus FIXED
public static final Network.ObjectStatus OVER_DEFINED
public static final Network.ObjectStatus NOT_CONSISTENT_DIMS
public static final Network.ObjectStatus NOT_CONSISTENT_OTHER
public static final Network.ObjectStatus NOT_CONSISTENT_UNKNOWN
public static final Network.ObjectStatus NOT_CHANGED
public static final Network.ObjectStatus WELL_DEFINED
public static final Network.ObjectStatus UNDER_DEFINED
public static final int _UNKNOWN
public static final int _FIXED
public static final int _OVER_DEFINED
public static final int _NOT_CONSISTENT_DIMS
public static final int _NOT_CONSISTENT_OTHER
public static final int _NOT_CONSISTENT_UNKNOWN
public static final int _NOT_CHANGED
public static final int _WELL_DEFINED
public static final int _UNDER_DEFINED
public static Network.ObjectStatus valueOf(int value)
public static Network.ObjectStatus valueOf(String name)
public static Network.ObjectStatus[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.