Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Field and Description |
---|---|
static Constraint.Type |
Constraint.Type.ALIGN_LOCK
Two geometries are constrained to have a common axis and no rotation about it
|
static Constraint.Type |
Constraint.Type.ANGLE
Two geometries have a specified angle between them
|
static Constraint.Type |
Constraint.Type.BALL
For internal use only
|
static Constraint.Type |
Constraint.Type.BOND
A number of movable objects form a rigid group
|
static Constraint.Type |
Constraint.Type.CABLE
For internal use only
|
static Constraint.Type |
Constraint.Type.CENTER12
One geometry is positioned mid-way between two others
|
static Constraint.Type |
Constraint.Type.CENTER22
An implicit plane between two geometries of one movable object is positioned mid-way between two others
|
static Constraint.Type |
Constraint.Type.CIRCULAR_PATTERN
For internal use only
|
static Constraint.Type |
Constraint.Type.COMMON_OFFSET_TRANSFORM
For internal use only
|
static Constraint.Type |
Constraint.Type.CONCENTRIC
Two geometries share a center and plane
|
static Constraint.Type |
Constraint.Type.CYLINDRICAL
For internal use only
|
static Constraint.Type |
Constraint.Type.DISTANCE
Two geometries have a specified distance between them
|
static Constraint.Type |
Constraint.Type.FIT
Two geometries are coincident
|
static Constraint.Type |
Constraint.Type.FIX
One movable object fixed
|
static Constraint.Type |
Constraint.Type.GEAR
For internal use only
|
static Constraint.Type |
Constraint.Type.HINGE
For internal use only
|
static Constraint.Type |
Constraint.Type.LINEAR_PATTERN
For internal use only
|
static Constraint.Type |
Constraint.Type.LINEAR2D_PATTERN
For internal use only
|
static Constraint.Type |
Constraint.Type.ORIENT_ANGLE
Two geometries have a specified angle between them about an axis
|
static Constraint.Type |
Constraint.Type.PARALLEL
Two geometries are parallel
|
static Constraint.Type |
Constraint.Type.PERPENDICULAR
Two geometries are perpendicular
|
static Constraint.Type |
Constraint.Type.RACK_PINION
For internal use only
|
static Constraint.Type |
Constraint.Type.RADIANT_PATTERN
For internal use only
|
static Constraint.Type |
Constraint.Type.SCREW
For internal use only
|
static Constraint.Type |
Constraint.Type.SLIDER
For internal use only
|
static Constraint.Type |
Constraint.Type.SPLINE_DATA
A spline and its defining points
|
static Constraint.Type |
Constraint.Type.SPLINE_LENGTH
Constrains the curve length of a spline
|
static Constraint.Type |
Constraint.Type.TOUCH
Two geometries touch
|
static Constraint.Type |
Constraint.Type.UNDEFINED
No type
|
Modifier and Type | Method and Description |
---|---|
Constraint.Type |
Constraint.constraintType()
Returns
the constraint type.
|
static Constraint.Type |
Constraint.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constraint.Type |
Constraint.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constraint.Type[] |
Constraint.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Constraint.setConstraintType(Constraint.Type constraintType)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.