public static class Constraint.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGN_LOCK
Two geometries are constrained to have a common axis and no rotation about it
|
static int |
_ANGLE
Two geometries have a specified angle between them
|
static int |
_BALL
For internal use only
|
static int |
_BOND
A number of movable objects form a rigid group
|
static int |
_CABLE
For internal use only
|
static int |
_CENTER12
One geometry is positioned mid-way between two others
|
static int |
_CENTER22
An implicit plane between two geometries of one movable object is positioned mid-way between two others
|
static int |
_CIRCULAR_PATTERN
For internal use only
|
static int |
_COMMON_OFFSET_TRANSFORM
For internal use only
|
static int |
_CONCENTRIC
Two geometries share a center and plane
|
static int |
_CYLINDRICAL
For internal use only
|
static int |
_DISTANCE
Two geometries have a specified distance between them
|
static int |
_FIT
Two geometries are coincident
|
static int |
_FIX
One movable object fixed
|
static int |
_GEAR
For internal use only
|
static int |
_HINGE
For internal use only
|
static int |
_LINEAR_PATTERN
For internal use only
|
static int |
_LINEAR2D_PATTERN
For internal use only
|
static int |
_ORIENT_ANGLE
Two geometries have a specified angle between them about an axis
|
static int |
_PARALLEL
Two geometries are parallel
|
static int |
_PERPENDICULAR
Two geometries are perpendicular
|
static int |
_RACK_PINION
For internal use only
|
static int |
_RADIANT_PATTERN
For internal use only
|
static int |
_SCREW
For internal use only
|
static int |
_SLIDER
For internal use only
|
static int |
_SPLINE_DATA
A spline and its defining points
|
static int |
_SPLINE_LENGTH
Constrains the curve length of a spline
|
static int |
_TOUCH
Two geometries touch
|
static int |
_UNDEFINED
No type
|
static Constraint.Type |
ALIGN_LOCK
Two geometries are constrained to have a common axis and no rotation about it
|
static Constraint.Type |
ANGLE
Two geometries have a specified angle between them
|
static Constraint.Type |
BALL
For internal use only
|
static Constraint.Type |
BOND
A number of movable objects form a rigid group
|
static Constraint.Type |
CABLE
For internal use only
|
static Constraint.Type |
CENTER12
One geometry is positioned mid-way between two others
|
static Constraint.Type |
CENTER22
An implicit plane between two geometries of one movable object is positioned mid-way between two others
|
static Constraint.Type |
CIRCULAR_PATTERN
For internal use only
|
static Constraint.Type |
COMMON_OFFSET_TRANSFORM
For internal use only
|
static Constraint.Type |
CONCENTRIC
Two geometries share a center and plane
|
static Constraint.Type |
CYLINDRICAL
For internal use only
|
static Constraint.Type |
DISTANCE
Two geometries have a specified distance between them
|
static Constraint.Type |
FIT
Two geometries are coincident
|
static Constraint.Type |
FIX
One movable object fixed
|
static Constraint.Type |
GEAR
For internal use only
|
static Constraint.Type |
HINGE
For internal use only
|
static Constraint.Type |
LINEAR_PATTERN
For internal use only
|
static Constraint.Type |
LINEAR2D_PATTERN
For internal use only
|
static Constraint.Type |
ORIENT_ANGLE
Two geometries have a specified angle between them about an axis
|
static Constraint.Type |
PARALLEL
Two geometries are parallel
|
static Constraint.Type |
PERPENDICULAR
Two geometries are perpendicular
|
static Constraint.Type |
RACK_PINION
For internal use only
|
static Constraint.Type |
RADIANT_PATTERN
For internal use only
|
static Constraint.Type |
SCREW
For internal use only
|
static Constraint.Type |
SLIDER
For internal use only
|
static Constraint.Type |
SPLINE_DATA
A spline and its defining points
|
static Constraint.Type |
SPLINE_LENGTH
Constrains the curve length of a spline
|
static Constraint.Type |
TOUCH
Two geometries touch
|
static Constraint.Type |
UNDEFINED
No type
|
Modifier and Type | Method and Description |
---|---|
static Constraint.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constraint.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constraint.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final Constraint.Type UNDEFINED
public static final Constraint.Type TOUCH
public static final Constraint.Type CONCENTRIC
public static final Constraint.Type FIX
public static final Constraint.Type DISTANCE
public static final Constraint.Type PARALLEL
public static final Constraint.Type PERPENDICULAR
public static final Constraint.Type CENTER12
public static final Constraint.Type CENTER22
public static final Constraint.Type ANGLE
public static final Constraint.Type FIT
public static final Constraint.Type BOND
public static final Constraint.Type ORIENT_ANGLE
public static final Constraint.Type SPLINE_DATA
public static final Constraint.Type SPLINE_LENGTH
public static final Constraint.Type LINEAR_PATTERN
public static final Constraint.Type CIRCULAR_PATTERN
public static final Constraint.Type LINEAR2D_PATTERN
public static final Constraint.Type RADIANT_PATTERN
public static final Constraint.Type ALIGN_LOCK
public static final Constraint.Type COMMON_OFFSET_TRANSFORM
public static final Constraint.Type HINGE
public static final Constraint.Type SLIDER
public static final Constraint.Type CYLINDRICAL
public static final Constraint.Type BALL
public static final Constraint.Type SCREW
public static final Constraint.Type GEAR
public static final Constraint.Type RACK_PINION
public static final Constraint.Type CABLE
public static final int _UNDEFINED
public static final int _TOUCH
public static final int _CONCENTRIC
public static final int _FIX
public static final int _DISTANCE
public static final int _PARALLEL
public static final int _PERPENDICULAR
public static final int _CENTER12
public static final int _CENTER22
public static final int _ANGLE
public static final int _FIT
public static final int _BOND
public static final int _ORIENT_ANGLE
public static final int _SPLINE_DATA
public static final int _SPLINE_LENGTH
public static final int _LINEAR_PATTERN
public static final int _CIRCULAR_PATTERN
public static final int _LINEAR2D_PATTERN
public static final int _RADIANT_PATTERN
public static final int _ALIGN_LOCK
public static final int _COMMON_OFFSET_TRANSFORM
public static final int _HINGE
public static final int _SLIDER
public static final int _CYLINDRICAL
public static final int _BALL
public static final int _SCREW
public static final int _GEAR
public static final int _RACK_PINION
public static final int _CABLE
public static Constraint.Type valueOf(int value)
public static Constraint.Type valueOf(String name)
public static Constraint.Type[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.