Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static Constraint.SplineType |
Constraint.SplineType.BY_POINTS
Spline points define interpolation/through points.
|
static Constraint.SplineType |
Constraint.SplineType.BY_POLES
Spline points define control points.
|
static Constraint.SplineType |
Constraint.SplineType.INVALID
Not a valid spline constraint.
|
Modifier and Type | Method and Description |
---|---|
Constraint.SplineType |
Constraint.splinePointsType()
Returns the type of the spline.
|
static Constraint.SplineType |
Constraint.SplineType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constraint.SplineType |
Constraint.SplineType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constraint.SplineType[] |
Constraint.SplineType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Constraint.setSplinePointsType(Constraint.SplineType splineType)
Sets the type of the spline.
|
Modifier and Type | Method and Description |
---|---|
void |
SplinePathBuilder.setSplineMethod(Constraint.SplineType splineMethod)
Deprecated.
Deprecated in NX11.0.2. Use
SplinePathBuilder.DefiningTypes instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.