Package | Description |
---|---|
nxopen.pid |
Provides classes and interfaces for PID.
|
Modifier and Type | Field and Description |
---|---|
static RotateAngleOption |
RotateAngleOption.NINETY
90 degree.
|
static RotateAngleOption |
RotateAngleOption.ONE_HUNDRED_AND_EIGHTY
180 degree.
|
static RotateAngleOption |
RotateAngleOption.TWO_HUNDRED_AND_SEVENTY
270 degree.
|
static RotateAngleOption |
RotateAngleOption.ZERO
0 degree.
|
Modifier and Type | Method and Description |
---|---|
RotateAngleOption |
EquipmentBuilder.rotate()
Returns the symbol rotation angle.
|
RotateAngleOption |
OffSheetConnectorBuilder.rotateOption()
Returns the symbol rotation angle.
|
static RotateAngleOption |
RotateAngleOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RotateAngleOption |
RotateAngleOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RotateAngleOption[] |
RotateAngleOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EquipmentBuilder.setRotate(RotateAngleOption rotate)
License requirements: nx_pid_design_author ("NX P and ID Design Author") . |
void |
OffSheetConnectorBuilder.setRotateOption(RotateAngleOption rotate)
License requirements: nx_pid_design_author ("NX P and ID Design Author") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.