public class RotateAngleOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NINETY
90 degree.
|
static int |
_ONE_HUNDRED_AND_EIGHTY
180 degree.
|
static int |
_TWO_HUNDRED_AND_SEVENTY
270 degree.
|
static int |
_ZERO
0 degree.
|
static RotateAngleOption |
NINETY
90 degree.
|
static RotateAngleOption |
ONE_HUNDRED_AND_EIGHTY
180 degree.
|
static RotateAngleOption |
TWO_HUNDRED_AND_SEVENTY
270 degree.
|
static RotateAngleOption |
ZERO
0 degree.
|
Modifier and Type | Method and Description |
---|---|
static RotateAngleOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RotateAngleOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RotateAngleOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final RotateAngleOption ZERO
public static final RotateAngleOption NINETY
public static final RotateAngleOption ONE_HUNDRED_AND_EIGHTY
public static final RotateAngleOption TWO_HUNDRED_AND_SEVENTY
public static final int _ZERO
public static final int _NINETY
public static final int _ONE_HUNDRED_AND_EIGHTY
public static final int _TWO_HUNDRED_AND_SEVENTY
public static RotateAngleOption valueOf(int value)
public static RotateAngleOption valueOf(String name)
public static RotateAngleOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.