Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
SensorsActuatorsListBuilder |
PhysicsManager.createSensorsActuatorsListBuilder()
Creates a
SensorsActuatorsListBuilder object. |
SensorsActuatorsListBuilder |
SensorsActuatorsListBuilderList.findItem(int index)
Returns the object at the input index.
|
SensorsActuatorsListBuilder[] |
SensorsActuatorsListBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SensorsActuatorsListBuilderList.append(SensorsActuatorsListBuilder object)
Appends an object to the list
License requirements: None. |
void |
SensorsActuatorsListBuilderList.append(SensorsActuatorsListBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SensorsActuatorsListBuilderList.erase(SensorsActuatorsListBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SensorsActuatorsListBuilderList.erase(SensorsActuatorsListBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SensorsActuatorsListBuilderList.findIndex(SensorsActuatorsListBuilder obj)
Finds the index where the input object appears.
|
void |
SensorsActuatorsListBuilderList.insert(int location,
SensorsActuatorsListBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SensorsActuatorsListBuilderList.setContents(SensorsActuatorsListBuilder[] objects)
Sets the contents of the entire list.
|
void |
SensorsActuatorsListBuilderList.swap(SensorsActuatorsListBuilder object1,
SensorsActuatorsListBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.