Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.CUSTOM
Custom that represents the user created temporary variable
|
ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.Slot.eSlotType
Slot type that indicate the data structure is used for
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.INPUT
Input that should connect to runtime parameter as input value.
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.NONE
None
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.NUM
Total Num
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.OUTPUT
Output that should connect to runtime parameter to output value
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.PARAM
Param that is used to configure the block to differentiate mode
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.STATE
State that is change during runtime based on internal data
|
Modifier and Type | Method and Description |
---|---|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExpressionBlockBuilder.SlotType |
ExpressionBlockBuilder.SlotType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExpressionBlockBuilder.SlotType[] |
ExpressionBlockBuilder.SlotType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Slot(ExpressionBlockBuilder.SlotType eSlotTypeInitial,
String nameInitial,
ExpressionBlockBuilder.DataType eDataTypeInitial,
boolean boolValueInitial,
int intValueInitial,
double doubleValueInitial,
Unit unitInitial,
String formulaInitial,
String commentInitial,
NXObject tgPhysicsObjectInitial,
int nPhysicsPropTagInitial)
Constructor for the Slot object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.