public static class ExpressionBlockBuilder.SlotType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUSTOM
Custom that represents the user created temporary variable
|
static int |
_INPUT
Input that should connect to runtime parameter as input value.
|
static int |
_NONE
None
|
static int |
_NUM
Total Num
|
static int |
_OUTPUT
Output that should connect to runtime parameter to output value
|
static int |
_PARAM
Param that is used to configure the block to differentiate mode
|
static int |
_STATE
State that is change during runtime based on internal data
|
static ExpressionBlockBuilder.SlotType |
CUSTOM
Custom that represents the user created temporary variable
|
static ExpressionBlockBuilder.SlotType |
INPUT
Input that should connect to runtime parameter as input value.
|
static ExpressionBlockBuilder.SlotType |
NONE
None
|
static ExpressionBlockBuilder.SlotType |
NUM
Total Num
|
static ExpressionBlockBuilder.SlotType |
OUTPUT
Output that should connect to runtime parameter to output value
|
static ExpressionBlockBuilder.SlotType |
PARAM
Param that is used to configure the block to differentiate mode
|
static ExpressionBlockBuilder.SlotType |
STATE
State that is change during runtime based on internal data
|
Modifier and Type | Method and Description |
---|---|
static ExpressionBlockBuilder.SlotType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExpressionBlockBuilder.SlotType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExpressionBlockBuilder.SlotType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExpressionBlockBuilder.SlotType NONE
public static final ExpressionBlockBuilder.SlotType INPUT
public static final ExpressionBlockBuilder.SlotType OUTPUT
public static final ExpressionBlockBuilder.SlotType PARAM
public static final ExpressionBlockBuilder.SlotType STATE
public static final ExpressionBlockBuilder.SlotType CUSTOM
public static final ExpressionBlockBuilder.SlotType NUM
public static final int _NONE
public static final int _INPUT
public static final int _OUTPUT
public static final int _PARAM
public static final int _STATE
public static final int _CUSTOM
public static final int _NUM
public static ExpressionBlockBuilder.SlotType valueOf(int value)
public static ExpressionBlockBuilder.SlotType valueOf(String name)
public static ExpressionBlockBuilder.SlotType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.