Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBoundingObjectBuilder |
TrimCurve2Builder.createTrimCurveBoundingObjectBuilder()
Creates an
TrimCurveBoundingObjectBuilder object. |
Modifier and Type | Method and Description |
---|---|
TrimCurveBoundingObjectBuilder |
TrimCurveBoundingObjectBuilderList.findItem(int index)
Returns the object at the input index.
|
TrimCurveBoundingObjectBuilder[] |
TrimCurveBoundingObjectBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBoundingObjectBuilderList.append(TrimCurveBoundingObjectBuilder object)
Appends an object to the list
License requirements: None. |
void |
TrimCurveBoundingObjectBuilderList.append(TrimCurveBoundingObjectBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TrimCurveBoundingObjectBuilderList.erase(TrimCurveBoundingObjectBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TrimCurveBoundingObjectBuilderList.erase(TrimCurveBoundingObjectBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TrimCurveBoundingObjectBuilderList.findIndex(TrimCurveBoundingObjectBuilder obj)
Finds the index where the input object appears.
|
void |
TrimCurveBoundingObjectBuilderList.insert(int location,
TrimCurveBoundingObjectBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TrimCurveBoundingObjectBuilderList.setContents(TrimCurveBoundingObjectBuilder[] objects)
Sets the contents of the entire list.
|
void |
TrimCurveBoundingObjectBuilderList.swap(TrimCurveBoundingObjectBuilder object1,
TrimCurveBoundingObjectBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.