Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
TransitionCurveBuilder |
Part.createEmptyTransitionCurveBuilder()
Creates a
TransitionCurveBuilder object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
TransitionCurveBuilder |
BlendCornerBuilder.createTransitionCurveBuilder()
Create a transition curve data builder object.
|
Modifier and Type | Method and Description |
---|---|
TransitionCurveBuilder |
TransitionCurveBuilderList.findItem(int index)
Returns the object at the input index.
|
TransitionCurveBuilder[] |
TransitionCurveBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TransitionCurveBuilderList.append(TransitionCurveBuilder object)
Appends an object to the list
License requirements: None. |
void |
TransitionCurveBuilderList.append(TransitionCurveBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TransitionCurveBuilderList.erase(TransitionCurveBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TransitionCurveBuilderList.erase(TransitionCurveBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TransitionCurveBuilderList.findIndex(TransitionCurveBuilder obj)
Finds the index where the input object appears.
|
void |
TransitionCurveBuilderList.insert(int location,
TransitionCurveBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TransitionCurveBuilderList.setContents(TransitionCurveBuilder[] objects)
Sets the contents of the entire list.
|
void |
TransitionCurveBuilderList.swap(TransitionCurveBuilder object1,
TransitionCurveBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.