Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
RotationSetBuilder |
StyledSweepBuilder.createRotationSet(double value,
double pathPar,
Curve path)
Creates a new rotation set
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
RotationSetBuilder |
RotationSetBuilderList.findItem(int index)
Returns the object at the input index.
|
RotationSetBuilder[] |
RotationSetBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
RotationSetBuilderList.append(RotationSetBuilder object)
Appends an object to the list
License requirements: None. |
void |
RotationSetBuilderList.append(RotationSetBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
RotationSetBuilderList.erase(RotationSetBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
RotationSetBuilderList.erase(RotationSetBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
RotationSetBuilderList.findIndex(RotationSetBuilder obj)
Finds the index where the input object appears.
|
void |
RotationSetBuilderList.insert(int location,
RotationSetBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
RotationSetBuilderList.setContents(RotationSetBuilder[] objects)
Sets the contents of the entire list.
|
void |
RotationSetBuilderList.swap(RotationSetBuilder object1,
RotationSetBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.