Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PatternOrientation.Enum |
PatternOrientation.Enum.CSYSTO_CSYS
a relative orientation defined by two CSYSs to transform the seed to an instance location.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.FIXED
same orientation as the seed.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.FOLLOW_CSYS
follow CSYS orientation, for general pattern type, when from/to is CSYS.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.FOLLOW_PATTERN
follow pattern orientation, for example, circular pattern type.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.NORMAL_TO_PATH
normal to path orientation for Along Type first direction.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.NORMAL_TO_VECTOR
normal to vector orientation for Along Type first direction.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.PARALLEL_TO_VECTOR
parallel to vector orientation for Along Type first direction.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.THROUGH_AXIS
through axis orientation for Along Type first direction.
|
Modifier and Type | Method and Description |
---|---|
PatternOrientation.Enum |
PatternOrientation.alongOrientationOption()
Returns the orientationOption for Along pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.circularOrientationOption()
Returns the orientationOption for Circular pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.generalOrientationOption()
Returns the orientationOption for General pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.helixOrientationOption()
Returns the orientationOption for Helix pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.linearOrientationOption()
Returns the orientationOption for Linear pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.mirrorOrientationOption()
Returns the orientationOption for Mirror pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.orientationOption()
Deprecated.
Deprecated in NX8.0.0. The replacement function depends on the pattern type. See this method's documentation for more detailed information.
|
PatternOrientation.Enum |
PatternOrientation.polygonOrientationOption()
Returns the orientationOption for Polygon pattern type
License requirements: None. |
PatternOrientation.Enum |
PatternOrientation.spiralOrientationOption()
Returns the orientationOption for Spiral pattern type
License requirements: None. |
static PatternOrientation.Enum |
PatternOrientation.Enum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternOrientation.Enum |
PatternOrientation.Enum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternOrientation.Enum[] |
PatternOrientation.Enum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternOrientation.setAlongOrientationOption(PatternOrientation.Enum alongOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setCircularOrientationOption(PatternOrientation.Enum circularOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setGeneralOrientationOption(PatternOrientation.Enum generalOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setHelixOrientationOption(PatternOrientation.Enum helixOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setLinearOrientationOption(PatternOrientation.Enum linearOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setMirrorOrientationOption(PatternOrientation.Enum mirrorOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setOrientationOption(PatternOrientation.Enum orientationOption)
Deprecated.
Deprecated in NX8.0.0. The replacement function depends on the pattern type. See this method's documentation for more detailed information.
|
void |
PatternOrientation.setPolygonOrientationOption(PatternOrientation.Enum polygonOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
PatternOrientation.setSpiralOrientationOption(PatternOrientation.Enum spiralOrientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.