public static class PatternOrientation.Enum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CSYSTO_CSYS
a relative orientation defined by two CSYSs to transform the seed to an instance location.
|
static int |
_FIXED
same orientation as the seed.
|
static int |
_FOLLOW_CSYS
follow CSYS orientation, for general pattern type, when from/to is CSYS.
|
static int |
_FOLLOW_PATTERN
follow pattern orientation, for example, circular pattern type.
|
static int |
_NORMAL_TO_PATH
normal to path orientation for Along Type first direction.
|
static int |
_NORMAL_TO_VECTOR
normal to vector orientation for Along Type first direction.
|
static int |
_PARALLEL_TO_VECTOR
parallel to vector orientation for Along Type first direction.
|
static int |
_THROUGH_AXIS
through axis orientation for Along Type first direction.
|
static PatternOrientation.Enum |
CSYSTO_CSYS
a relative orientation defined by two CSYSs to transform the seed to an instance location.
|
static PatternOrientation.Enum |
FIXED
same orientation as the seed.
|
static PatternOrientation.Enum |
FOLLOW_CSYS
follow CSYS orientation, for general pattern type, when from/to is CSYS.
|
static PatternOrientation.Enum |
FOLLOW_PATTERN
follow pattern orientation, for example, circular pattern type.
|
static PatternOrientation.Enum |
NORMAL_TO_PATH
normal to path orientation for Along Type first direction.
|
static PatternOrientation.Enum |
NORMAL_TO_VECTOR
normal to vector orientation for Along Type first direction.
|
static PatternOrientation.Enum |
PARALLEL_TO_VECTOR
parallel to vector orientation for Along Type first direction.
|
static PatternOrientation.Enum |
THROUGH_AXIS
through axis orientation for Along Type first direction.
|
Modifier and Type | Method and Description |
---|---|
static PatternOrientation.Enum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternOrientation.Enum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternOrientation.Enum[] |
values()
Returns an array that contains the values for this enum.
|
public static final PatternOrientation.Enum FIXED
public static final PatternOrientation.Enum NORMAL_TO_PATH
public static final PatternOrientation.Enum NORMAL_TO_VECTOR
public static final PatternOrientation.Enum PARALLEL_TO_VECTOR
public static final PatternOrientation.Enum THROUGH_AXIS
public static final PatternOrientation.Enum FOLLOW_PATTERN
public static final PatternOrientation.Enum FOLLOW_CSYS
public static final PatternOrientation.Enum CSYSTO_CSYS
public static final int _FIXED
public static final int _NORMAL_TO_PATH
public static final int _NORMAL_TO_VECTOR
public static final int _PARALLEL_TO_VECTOR
public static final int _THROUGH_AXIS
public static final int _FOLLOW_PATTERN
public static final int _FOLLOW_CSYS
public static final int _CSYSTO_CSYS
public static PatternOrientation.Enum valueOf(int value)
public static PatternOrientation.Enum valueOf(String name)
public static PatternOrientation.Enum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.