Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.AnchorPositionType.CENTER
Anchor at the center of the curve
|
static CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.AnchorPositionType.END
Anchor at the end of the curve
|
static CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.AnchorPositionType.START
Anchor at the start of the curve
|
Modifier and Type | Method and Description |
---|---|
CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.anchorPosition()
Returns the anchor position
License requirements: None. |
static CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.AnchorPositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveRangeBuilder.AnchorPositionType |
CurveRangeBuilder.AnchorPositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveRangeBuilder.AnchorPositionType[] |
CurveRangeBuilder.AnchorPositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveRangeBuilder.setAnchorPosition(CurveRangeBuilder.AnchorPositionType anchorPosition)
Sets the anchor position
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.