public static class CurveRangeBuilder.AnchorPositionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CENTER
Anchor at the center of the curve
|
static int |
_END
Anchor at the end of the curve
|
static int |
_START
Anchor at the start of the curve
|
static CurveRangeBuilder.AnchorPositionType |
CENTER
Anchor at the center of the curve
|
static CurveRangeBuilder.AnchorPositionType |
END
Anchor at the end of the curve
|
static CurveRangeBuilder.AnchorPositionType |
START
Anchor at the start of the curve
|
Modifier and Type | Method and Description |
---|---|
static CurveRangeBuilder.AnchorPositionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveRangeBuilder.AnchorPositionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveRangeBuilder.AnchorPositionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CurveRangeBuilder.AnchorPositionType START
public static final CurveRangeBuilder.AnchorPositionType CENTER
public static final CurveRangeBuilder.AnchorPositionType END
public static final int _START
public static final int _CENTER
public static final int _END
public static CurveRangeBuilder.AnchorPositionType valueOf(int value)
public static CurveRangeBuilder.AnchorPositionType valueOf(String name)
public static CurveRangeBuilder.AnchorPositionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.