Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static CurveOptions.InputCurve |
CurveOptions.InputCurve.BLANK
Blanks the original input curve and creates the new output curve
|
static CurveOptions.InputCurve |
CurveOptions.InputCurve.DELETE
Deletes the original input curve and creates the new output curve
|
static CurveOptions.InputCurve |
CurveOptions.InputCurve.REPLACE
Replaces the original input curve with the new output curve
|
static CurveOptions.InputCurve |
CurveOptions.InputCurve.RETAIN
Retains the original input curve and creates the new output curve
|
Modifier and Type | Method and Description |
---|---|
CurveOptions.InputCurve |
CurveOptions.inputCurveOption()
Returns the curve options
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
static CurveOptions.InputCurve |
CurveOptions.InputCurve.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveOptions.InputCurve |
CurveOptions.InputCurve.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveOptions.InputCurve[] |
CurveOptions.InputCurve.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveOptions.setInputCurveOption(CurveOptions.InputCurve inputCurveOption)
Sets the curve options
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.