Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeBlendBuilder.removeStopshortDataByType(Edge edge,
boolean fromStart,
BlendStopshortBuilder.Choices type)
Remove the stop short from an edge, given its type and location
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Field and Description |
---|---|
static BlendStopshortBuilder.Choices |
BlendStopshortBuilder.Choices.AT_DISTANCE
Distance
|
static BlendStopshortBuilder.Choices |
BlendStopshortBuilder.Choices.AT_INTERSECTION
Intersection
|
Modifier and Type | Method and Description |
---|---|
BlendStopshortBuilder.Choices |
BlendStopshortBuilder.choice()
Returns the Stopshort option choice.
|
static BlendStopshortBuilder.Choices |
BlendStopshortBuilder.Choices.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlendStopshortBuilder.Choices |
BlendStopshortBuilder.Choices.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlendStopshortBuilder.Choices[] |
BlendStopshortBuilder.Choices.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
BlendStopshortBuilder |
BlendStopshortBuilderCollection.create(BlendStopshortBuilder.Choices mChoice,
Expression mOnPathExp,
Edge mPath,
boolean mIsFlipped,
Point mThruPoint)
Creates an BlendStopshortBuilder.
|
void |
BlendStopshortBuilder.setChoice(BlendStopshortBuilder.Choices mChoice)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.