Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BlendSetbackBuilder.Directions |
BlendSetbackBuilder.Directions.PLANE
setback curve is the intersection curve between a plane and faces
|
static BlendSetbackBuilder.Directions |
BlendSetbackBuilder.Directions.U
setback curve is an iso-u parameter curve
|
static BlendSetbackBuilder.Directions |
BlendSetbackBuilder.Directions.V
setback curve is an iso-v parameter curve
|
Modifier and Type | Method and Description |
---|---|
BlendSetbackBuilder.Directions |
BlendSetbackBuilder.direction()
Returns the direction type
License requirements: None. |
static BlendSetbackBuilder.Directions |
BlendSetbackBuilder.Directions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlendSetbackBuilder.Directions |
BlendSetbackBuilder.Directions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlendSetbackBuilder.Directions[] |
BlendSetbackBuilder.Directions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BlendSetbackBuilder.setDirection(BlendSetbackBuilder.Directions direction)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.