public static class BlendSetbackBuilder.Directions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PLANE
setback curve is the intersection curve between a plane and faces
|
static int |
_U
setback curve is an iso-u parameter curve
|
static int |
_V
setback curve is an iso-v parameter curve
|
static BlendSetbackBuilder.Directions |
PLANE
setback curve is the intersection curve between a plane and faces
|
static BlendSetbackBuilder.Directions |
U
setback curve is an iso-u parameter curve
|
static BlendSetbackBuilder.Directions |
V
setback curve is an iso-v parameter curve
|
Modifier and Type | Method and Description |
---|---|
static BlendSetbackBuilder.Directions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlendSetbackBuilder.Directions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlendSetbackBuilder.Directions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BlendSetbackBuilder.Directions U
public static final BlendSetbackBuilder.Directions V
public static final BlendSetbackBuilder.Directions PLANE
public static final int _U
public static final int _V
public static final int _PLANE
public static BlendSetbackBuilder.Directions valueOf(int value)
public static BlendSetbackBuilder.Directions valueOf(String name)
public static BlendSetbackBuilder.Directions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.