Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static AlongSpineBuilder.RetainSpineOption |
AlongSpineBuilder.RetainSpineOption.KEEP_ORIGINAL
Keeps the original profile as it is during edit of pre NX3 parms
|
static AlongSpineBuilder.RetainSpineOption |
AlongSpineBuilder.RetainSpineOption.REPLACE
Deletes the old profile, so that user has to select new one during edit of pre NX3 parms
|
Modifier and Type | Method and Description |
---|---|
AlongSpineBuilder.RetainSpineOption |
AlongSpineBuilder.spineOption()
Returns the alongSpineOption.
|
static AlongSpineBuilder.RetainSpineOption |
AlongSpineBuilder.RetainSpineOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongSpineBuilder.RetainSpineOption |
AlongSpineBuilder.RetainSpineOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongSpineBuilder.RetainSpineOption[] |
AlongSpineBuilder.RetainSpineOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AlongSpineBuilder.setSpineOption(AlongSpineBuilder.RetainSpineOption spineOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.