public static class AlongSpineBuilder.RetainSpineOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_KEEP_ORIGINAL
Keeps the original profile as it is during edit of pre NX3 parms
|
static int |
_REPLACE
Deletes the old profile, so that user has to select new one during edit of pre NX3 parms
|
static AlongSpineBuilder.RetainSpineOption |
KEEP_ORIGINAL
Keeps the original profile as it is during edit of pre NX3 parms
|
static AlongSpineBuilder.RetainSpineOption |
REPLACE
Deletes the old profile, so that user has to select new one during edit of pre NX3 parms
|
Modifier and Type | Method and Description |
---|---|
static AlongSpineBuilder.RetainSpineOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongSpineBuilder.RetainSpineOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongSpineBuilder.RetainSpineOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlongSpineBuilder.RetainSpineOption KEEP_ORIGINAL
public static final AlongSpineBuilder.RetainSpineOption REPLACE
public static final int _KEEP_ORIGINAL
public static final int _REPLACE
public static AlongSpineBuilder.RetainSpineOption valueOf(int value)
public static AlongSpineBuilder.RetainSpineOption valueOf(String name)
public static AlongSpineBuilder.RetainSpineOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.