Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static AlongPathPattern.PathOptions |
AlongPathPattern.PathOptions.OFFSET
path is an offset from the selected path.
|
static AlongPathPattern.PathOptions |
AlongPathPattern.PathOptions.RIGID
path is the selected section.
|
static AlongPathPattern.PathOptions |
AlongPathPattern.PathOptions.TRANSLATE
path is a translation from the selected path.
|
Modifier and Type | Method and Description |
---|---|
static AlongPathPattern.PathOptions |
AlongPathPattern.PathOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongPathPattern.PathOptions |
AlongPathPattern.PathOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongPathPattern.PathOptions[] |
AlongPathPattern.PathOptions.values()
Returns an array that contains the values for this enum.
|
AlongPathPattern.PathOptions |
AlongPathPattern.xpathOption()
Returns the x path options
License requirements: None. |
AlongPathPattern.PathOptions |
AlongPathPattern.ypathOption()
Returns the y path options
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
AlongPathPattern.setXPathOption(AlongPathPattern.PathOptions xPathOption)
License requirements: None. |
void |
AlongPathPattern.setYPathOption(AlongPathPattern.PathOptions yPathOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.