public static class AlongPathPattern.PathOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OFFSET
path is an offset from the selected path.
|
static int |
_RIGID
path is the selected section.
|
static int |
_TRANSLATE
path is a translation from the selected path.
|
static AlongPathPattern.PathOptions |
OFFSET
path is an offset from the selected path.
|
static AlongPathPattern.PathOptions |
RIGID
path is the selected section.
|
static AlongPathPattern.PathOptions |
TRANSLATE
path is a translation from the selected path.
|
Modifier and Type | Method and Description |
---|---|
static AlongPathPattern.PathOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongPathPattern.PathOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongPathPattern.PathOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlongPathPattern.PathOptions RIGID
public static final AlongPathPattern.PathOptions OFFSET
public static final AlongPathPattern.PathOptions TRANSLATE
public static final int _RIGID
public static final int _OFFSET
public static final int _TRANSLATE
public static AlongPathPattern.PathOptions valueOf(int value)
public static AlongPathPattern.PathOptions valueOf(String name)
public static AlongPathPattern.PathOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.