Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.LineOrientationType.BOTH
Both horizontal and vertical.
|
static ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.LineOrientationType.HORIZONTAL
Horizontal.
|
static ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.LineOrientationType.VERTICAL
Vertical.
|
Modifier and Type | Method and Description |
---|---|
ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.lineOrientation()
Returns the reflection line orientation.
|
static ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.LineOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReflectionAnalysisBuilder.LineOrientationType |
ReflectionAnalysisBuilder.LineOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReflectionAnalysisBuilder.LineOrientationType[] |
ReflectionAnalysisBuilder.LineOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReflectionAnalysisBuilder.setLineOrientation(ReflectionAnalysisBuilder.LineOrientationType lineOrientation)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.