public static class ReflectionAnalysisBuilder.LineOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH
Both horizontal and vertical.
|
static int |
_HORIZONTAL
Horizontal.
|
static int |
_VERTICAL
Vertical.
|
static ReflectionAnalysisBuilder.LineOrientationType |
BOTH
Both horizontal and vertical.
|
static ReflectionAnalysisBuilder.LineOrientationType |
HORIZONTAL
Horizontal.
|
static ReflectionAnalysisBuilder.LineOrientationType |
VERTICAL
Vertical.
|
Modifier and Type | Method and Description |
---|---|
static ReflectionAnalysisBuilder.LineOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReflectionAnalysisBuilder.LineOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReflectionAnalysisBuilder.LineOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ReflectionAnalysisBuilder.LineOrientationType HORIZONTAL
public static final ReflectionAnalysisBuilder.LineOrientationType VERTICAL
public static final ReflectionAnalysisBuilder.LineOrientationType BOTH
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _BOTH
public static ReflectionAnalysisBuilder.LineOrientationType valueOf(int value)
public static ReflectionAnalysisBuilder.LineOrientationType valueOf(String name)
public static ReflectionAnalysisBuilder.LineOrientationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.