Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
nxopen.geometricanalysis.sectionanalysis |
Provides classes and interfaces for Section Analysis.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CurveContinuity
Represents a Curve Continuity Analysis builder
To create or edit an instance of this class, use CurveContinuityBuilder Created in NX7.0.0 |
interface |
CurveCurvatureAnalysis
Represents a CurveCurvatureAnalysis builder
To create or edit an instance of this class, use CurveCurvatureAnalysisBuilder Created in NX7.0.0 |
interface |
DeviationGauge
Deviation Gauge analysis object class
To create or edit an instance of this class, use DeviationGaugeBuilder Created in NX6.0.0 |
interface |
DraftAnalysis
Represents a Draft Analysis builder
To create or edit an instance of this class, use DraftAnalysisBuilder Created in NX8.0.0 |
interface |
FaceAnalysis
Represents a face analysis
To create or edit an instance of this class, use ReflectionAnalysisBuilder Created in NX11.0.0 |
interface |
FaceCurvatureAnalysis
Represents a Face Curvature Analysis builder
To create or edit an instance of this class, use FaceCurvatureAnalysisBuilder Created in NX8.0.0 |
interface |
GapFlushness
Gap and Flushness analysis object class
To create or edit an instance of this class, use GapFlushnessBuilder Created in NX5.0.0 |
interface |
HighlightLinesAnalysis
Represents a Highlight Lines Analysis object.
|
interface |
LocalRadiusAnalysis
Builder for Local Radius Analysis (formerly Dynamic Radius)
To create or edit an instance of this class, use LocalRadiusAnalysisBuilder Created in NX8.5.0 |
interface |
SectionAnalysisObject
Represents a Section Analysis object.
|
interface |
SurfaceContinuityAnalysis
Represents a SurfaceContinuityAnalysis builder
To create or edit an instance of this class, use SurfaceContinuityAnalysisBuilder Created in NX6.0.0 |
interface |
SurfaceIntersection
Represents a SurfaceIntersection builder
To create or edit an instance of this class, use SurfaceIntersectionBuilder Created in NX7.5.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
SectionAnalysisExObject
Represents a Section Analysis Object of the new version.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DieEngTrimAngleCheck
Represents a die engineering trim angle check analysis object
To create or edit an instance of this class, use DieEngTrimAngleCheckBuilder Created in NX8.5.0 |
Modifier and Type | Method and Description |
---|---|
DieEngTrimAngleCheckBuilder |
AutoDieCollection.createDieEngTrimAngleCheckBuilder(AnalysisObject dieEngTrimAngleCheck)
Creates a Die Engineering Trim Angle Check builder
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.