Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.Types.CGM_FILE_SELECTION
Import CGM file by browsing a CGM file
|
static FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.Types.COMPONENT_ATTRIBUTE
Import CGM file by selecting a component
|
static FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.Types.PATTERN_FILE_SELECTION
Import a pattern file
|
Modifier and Type | Method and Description |
---|---|
FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.type()
Returns the
FaceAnnotationBuilder.Types
selected by user
License requirements: routing_harness ("Routing Harness") Created in NX7.5.0 |
static FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceAnnotationBuilder.Types |
FaceAnnotationBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceAnnotationBuilder.Types[] |
FaceAnnotationBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceAnnotationBuilder.setType(FaceAnnotationBuilder.Types type)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.