Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static FaceAnnotationBuilder.DrwDestination |
FaceAnnotationBuilder.DrwDestination.DRAWING_SHEET
Place geometry in drawing sheet
|
static FaceAnnotationBuilder.DrwDestination |
FaceAnnotationBuilder.DrwDestination.MODEL
Place geometry in model
|
Modifier and Type | Method and Description |
---|---|
FaceAnnotationBuilder.DrwDestination |
FaceAnnotationBuilder.destEnum()
Returns the
FaceAnnotationBuilder.DrwDestination selected by
user to place the geometry
License requirements: routing_harness ("Routing Harness") Created in NX7.5.0 |
static FaceAnnotationBuilder.DrwDestination |
FaceAnnotationBuilder.DrwDestination.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceAnnotationBuilder.DrwDestination |
FaceAnnotationBuilder.DrwDestination.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceAnnotationBuilder.DrwDestination[] |
FaceAnnotationBuilder.DrwDestination.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceAnnotationBuilder.setDestEnum(FaceAnnotationBuilder.DrwDestination destEnum)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.