Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.CONSTANT
Returns the boundary value as interpolation result
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.CUBIC
Extrapolates from the boundary out into space using the cubic extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.EXTRAPOLATE
Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.LINEAR
Extrapolates from the boundary out into space using the linear extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.PARABOLIC
Extrapolates from the boundary out into space using the parabolic extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.UNDEFINED
No interpolation result
|
Modifier and Type | Method and Description |
---|---|
FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldReference.getSecondaryValuesOutsideTableInterpolation()
If the reference field is heterogeneous, set the outside table values interpolation method for the secondary independent domain .
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum[] |
FieldEvaluator.ValuesOutsideTableInterpolationEnum.values()
Returns an array that contains the values for this enum.
|
FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldTable.valuesOutsideTableInterpolation()
Returns the outside table values interpolation method for standard linear interpolation
License requirements: None. |
FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldReference.valuesOutsideTableInterpolation()
Returns the outside table values interpolation method for linear interpolation.
|
FieldEvaluator.ValuesOutsideTableInterpolationEnum |
FieldLinksTable.valuesOutsideTableInterpolation()
Returns the outside table values interpolation method for linear interpolation
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
FieldReference |
FieldManager.createProfileExternalTable(String fieldName,
String filePath,
int nbAbscisae,
int xColumn,
int yColumn,
int ordinateColumn,
Expression xOffset,
Expression yOffset,
Expression ordinateOffset,
Expression xScale,
Expression yScale,
Expression ordinateScale,
boolean xCyclic,
boolean yCyclic,
FieldEvaluator.InterpolationEnum interpolation,
FieldEvaluator.ValuesOutsideTableInterpolationEnum xExtrapolation,
FieldEvaluator.ValuesOutsideTableInterpolationEnum yExtrapolation,
Expression slopeLeft,
Expression slopeRight)
Creates an External Data Table Profile
License requirements: None. |
void |
FieldManager.editProfileExternalTable(FieldReference externalFileRefField,
String fieldName,
String filePath,
int nbAbscisae,
int xColumn,
int yColumn,
int ordinateColumn,
Expression xOffset,
Expression yOffset,
Expression ordinateOffset,
Expression xScale,
Expression yScale,
Expression ordinateScale,
boolean xCyclic,
boolean yCyclic,
FieldEvaluator.InterpolationEnum interpolation,
FieldEvaluator.ValuesOutsideTableInterpolationEnum xExtrapolation,
FieldEvaluator.ValuesOutsideTableInterpolationEnum yExtrapolation,
Expression slopeLeft,
Expression slopeRight)
Modifies an External Data Table Profile
License requirements: None. |
void |
FieldReference.setSecondaryValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
If the reference field is heterogeneous, set the outside table values interpolation method for the secondary independent domain .
|
void |
FieldLinksTable.setSecondaryValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
Set the values outside table interpolation option for sub fields if the sub fields are tables
License requirements: None. |
void |
FieldTable.setValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
License requirements: None. |
void |
FieldReference.setValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
License requirements: None. |
void |
FieldLinksTable.setValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.